Commands are listed here with transfer parameters that the visualization processes when an input event occurs.
|
“Configure commands” |
![]()
Click the |
![]() |
The command in “Configure commands” is added to the list. |
![]() |
The command is removed. Requirement: A command is selected. |
|
The order in the list defines the order of execution. |
|
![]() |
The selected command is moved down one position in the list. |
![]() |
The selected command is moved up one position in the list. |
|
“Command” |
“1st parameter” |
“2nd parameter” |
|
|
|
|
|
EXE file that is executed on the controller The program is executed on the PLC and therefore it must not be interactive or have any user interfaces. It is possible, for example, for a program to copy a file. |
Program name with directory as a string in single straight quotation marks |
Arguments of the program as a string in single straight quotation marks Example: Name of the file that the program opens |
|
“Command” |
“1. Parameters” |
“2. Parameters” |
|
|
|
|
|
EXE file that is executed on the display variant. Exception: WebVisu. The program is executed within the context of the display variant. After this, the program may be interactive and have a user interface. |
Program name with directory as |
Arguments of the program as Example: Name of the file that the program opens |




NOTICE

If the visualization is displayed as a CODESYS WebVisu, then no program (EXE file) can be started.
|
“Command” |
“1. Parameters” |
“2. Parameters” |
|
|
|
|
|
The visualization navigates to the web page of the URL. Requirement: The visualization is executed as a CODESYS WebVisu. |
URL
|
If a parameter is not specified, then the web page is displayed in a new window or a new tab. If |
|
“Command” |
“1st parameter” |
“2nd parameter” |
|
|
|
|
|
Name of the recipe definition
|
Name of the recipe
|
|
|
At visualization runtime, the controller reads the actual values from the variables of the recipe definition and writes them to the specified recipe. The values are saved implicitly (to a file on the controller) and shown in the recipe definition in the Recipe Manager of CODESYS. In other words, the recipe which is managed in CODESYS is updated with values from the controller. |
||
|
“Command” |
“1. Parameters” |
“2. Parameters” |
|
|
|
|
|
Name of the affected recipe definition
|
Name of the recipe (from the recipe definition)
|
|
|
At visualization runtime, the values of the recipe are written to the variables on the controller as they are in the Recipe Manager. |
||
|
“Command” |
“1. Parameters” |
“2. Parameters” |
|
|
|
|
|
Name of the affected recipe definition
|
Name of the affected recipe that is updated and saved to a file
Optional parameter: If you do not specify a transfer parameter here, then the values from the recipe variables are saved only the file that is specified later. The implicit recipe files are not updated. |
|
|
At visualization runtime, the “Save Recipe as” dialog opens and prompts the user for a file name and a storage location on the controller.
The file name must not be The user can then save the file that includes the actual values from the recipe variables. If a transfer parameter is not specified in the 2nd parameter, then the file is saved without changing an implicit recipe file. If a transfer parameter is given in the 2nd parameter, then the implicit recipe file is also updated. Note: If the “Save recipe changes to recipe files automatically” option is selected in the “Recipe Manager – General” tab, then the recipe definition in CODESYS and the implicit recipe files are kept the same automatically. Note: Implicit (automatically generated) recipe files exist on the controller with
names in the following syntax: |
||
|
“Command” |
“1st parameter” |
“2nd parameter” |
|
|
|
|
|
Name of the affected recipe definition
|
Name of the affected recipe
|
|
|
At visualization runtime, the “Load Recipe” dialog opens. It provides the visualization user with a file list that is located
in the file system of the controller and filters by the extension Requirement: The file was created with the |
||
|
“Command” |
“1. Parameters” |
“2. Parameters” |
|
|
|
|
|
Name of the affected recipe definition
|
Name of the new recipe
|
|
|
At visualization runtime, a new recipe is created in the given recipe definition. |
||
|
“Command” |
“1. Parameters” |
“2. Parameters” |
|
|
|
|
|
Name of the affected recipe definition
|
Name of the recipe
|
|
|
At visualization runtime, the specified recipe is deleted from the recipe definition. |
||

symbol to add the selected command to the lower command list.